Other Parts Discussed in Thread: TCA9548A
求助 TCA9548A可以进行级联使用吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TCA9548A
求助 TCA9548A可以进行级联使用吗
你好 我将两个TCA9548A进行级联以后 用端口检索程序检索不到第二片TCA9548A的地址 两片芯片没有问题
/**
* TCA9548 I2CScanner.pde -- I2C bus scanner for Arduino
*
* Based on code c. 2009, Tod E. Kurt, http://todbot.com/blog/
*
*/
#include "Wire.h"
extern "C" {
#include "utility/twi.h" // from Wire library, so we can do bus scanning
}
#define TCAADDR 0x70
void tcaselect(uint8_t i) {
if (i > 7) return;
Wire.beginTransmission(TCAADDR);
Wire.write(1 << i);
Wire.endTransmission();
}
// standard Arduino setup()
void setup()
{
while (!Serial);
delay(1000);
Wire.begin();
Serial.begin(115200);
Serial.println("\nTCAScanner ready!");
for (uint8_t t=0; t<8; t++) {
tcaselect(t);
Serial.print("TCA Port #"); Serial.println(t);
for (uint8_t addr = 0; addr<=127; addr++) {
if (addr == TCAADDR) continue;
uint8_t data;
if (! twi_writeTo(addr, &data, 0, 1, 1)) {
Serial.print("Found I2C 0x"); Serial.println(addr,HEX);
}
}
}
Serial.println("\ndone");
}
void loop()
{
}