This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940解調問題

HI,

想請問下DS90UB940解出的MIPI  8个数据+2个时钟是复制输出还是奇偶关系?

謝謝

  • 您好,要看您是哪种应用,UB940 可以配置为以下几种应用模式, 最后一种为复制输出。
    The device can be configured in following modes:
    • 1-lane FPD-Link III Input, 4 MIPI lanes Output
    • 1-lane FPD-Link III Input, 2 MIPI lanes Output
    • 2-lane FPD-Link III Input, 4 MIPI lanes Output
    • 2-lane FPD-Link III Input, 4 MIPI lanes Output
    • 1- or 2-lane FPD-Link III Input, 2 or 4 MIPI lanes Output (Replicate)