Other Parts Discussed in Thread: LMH0044, LMH0318, LMH0056
Dear all,
如下图,若实现以下功能,LMH0044和LMH0318是否可以实现?
1、视频源是1路AV信号和1路3G-SDI信号;
2、输出是一路3G-SDI信号;
3、通过控制切换信号选择AV或者3G-SDI视频信号输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为您上面提到AV转SDI 功能,所以我现在需要和您确认下您的应用,也就是说现在视频源一路AV,一路SDI,然后选择一款开关器件,选通SDI输出是吗?
{Dear Kailyn,
感谢您的回复;
若使用LMH0056配合LMH0044是否可以实现双路SDI选通和AV转SDI的功能?}
您好,很抱歉我们没有开关器件支持SDI和AV信号的切换。
建议的方案是您使用FPGA,有模拟接口接AV信号,另外FPGA的IP core 支持SDI信号,所以可以考虑使用FPGA 同时接AV和SDI信号。