This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

953和954通信 i2c no ack

1、问题现象:相机用953和954这一对串化器连接

相机反复重启会有启动失败情况(不出图黑屏)、反复重启30次左右、会出现2次失败

log里面显示 no ack

逻辑分析仪波形分析

可能是954那端并没有发送任何数据 、953那边多发出来一个字节  0x42导致、同时发送的0x42也没有时许也不对,时间间隔很短

请帮忙分析一下原因、

I2C波形正常

camera上电时序正常

通过逻辑分析仪抓取953和954两端的i2c数据波形如图所示(相机启动失败)

正常情况下(相机启动正常)