This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550 如何配置并送收 CANFD bus 信号?



目前根据 TCAN455x Driver Library Demo_1.2.1_manifest.html demo 进行修改,跑出 500K 的 CAN bus 送收资料,在 CAN FD bus 的送收上一直实现不了,芯片初始化配置是采用 Init_CAN();函数来进行的,与 CAN FD 相关的初始化配置如下:

#if 1
   /* Configure the CAN bus speeds */
   TCAN4x5x_MCAN_Nominal_Timing_Simple TCANNomTiming = {0}; // 500k arbitration with a 40 MHz crystal ((40E6 / 2) / (32 + 8) = 500E3)
   TCANNomTiming.NominalBitRatePrescaler = 2;       // 标称比特率预分频器
   TCANNomTiming.NominalTqBeforeSamplePoint = 32;   // 采样点之前的标称时间段
   TCANNomTiming.NominalTqAfterSamplePoint = 8;     // 采样点后的标称时间段
#else
   /* Configure the CAN bus speeds */
   TCAN4x5x_MCAN_Nominal_Timing_Simple TCANNomTiming = {0}; // 500k arbitration with a 40 MHz crystal ((40E6 / 2) / (32 + 8) = 500E3)
   TCANNomTiming.NominalBitRatePrescaler = 1;
   TCANNomTiming.NominalTqBeforeSamplePoint = 15;
   TCANNomTiming.NominalTqAfterSamplePoint = 5;
#endif
   TCAN4x5x_MCAN_Data_Timing_Simple TCANDataTiming = {0};  // 2 Mbps CAN FD with a 40 MHz crystal (40E6 / (15 + 5) = 2E6)
   TCANDataTiming.DataBitRatePrescaler = 1;
   TCANDataTiming.DataTqBeforeSamplePoint = 15;
   TCANDataTiming.DataTqAfterSamplePoint = 5;
   /* Configure the MCAN core settings */
   TCAN4x5x_MCAN_CCCR_Config cccrConfig = {0};     // Remember to initialize to 0, or you'll get random garbage!
   cccrConfig.FDOE = 1;          // CAN FD mode enable
   cccrConfig.BRSE = 1;          // CAN FD Bit rate switch enable
这样配置跑出来的通信都是 CAN bus 的 500K,请问这是什么原因造成的呢?