This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954怎么将CSI中的RX0和RX1的两个通道的数据分离

DS90UB954同时接两个ADAS摄像头模组的情况下,PORT0 PORT1都使能了,在CSI-PORT0 和 CSI-PORT1有信号输出,手册上介绍说CSI-PORT0中的信号也包含CSI-PORT1的信号,那么怎么将这两个CSI信号分离开?分别输出两张图

  • 您好,

    感谢您使用E2EChina 论坛。您的问题我正在处理,我会尽快回复您。
  • 您好,CSI2中的信号由MIPI规范中定义的虚拟通道号分开,您可以查看寄存器0x70/71/72的VC number设置。此外,这由下游SOC确定。 (The signals in CSI2 port are separated by virtual channel number defined in MIPI spec., you can check reg. 0x70/71/72 on VC number setting. Also, this is identified by the downstream SOC.)