This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571锁定问题



你好!

我们用的内部VCO,参考输入是16.8MHz,目标是让芯片输出某些频点的单载波(无调制)。发现芯片输出100M至600M大部分频点都很好,但是在若干频率附近就不能稳定LOCK。不能稳定锁定的频点频谱也很宽,能锁定的频谱很纯净。

比如在385MHz能锁定,寄存器值(R0~R7):

0x0083, 0x0101, 0x1e75, 0x3880, 0x3016, 0x0101, 0x8686, 0x09c4

 但在384MHz不能稳定锁定,寄存器值(R0~R7):

0x0083, 0x0100, 0xd055, 0x3880, 0x301a, 0x0101, 0x8786, 0x09c4

黄色是不同的寄存器值。我从200M,每隔1M一直测试到600M,对比多个锁定和不锁定的相邻频点,发现CHDIV1都刚好改变了。

请帮忙查下,谢谢!