This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn74lvc8t245输出漏电流问题

Other Parts Discussed in Thread: SN74LVC8T245, SN74LVC8T245-Q1

你好,目前我使用了sn74lvc8t245的电平转换芯片,3.3V与5V间互转。VCCA=3.3V。5V的输出信号通过连接器到光耦部分,目前连接器没有接,相当于是开路的。我这边实测5V部分电流消耗了18mA(即R83那一路)。我看规格书描述不应该是20uA吗?后来通过连接器连上光耦部分,电流变成了0.18mA,也与规格书不符。都是在使能端为高电平情况下测试,即芯片左右两边是不通的。

  • 您好,

    规格书里描述的20uA,您指的是哪个参数呢

    OE为高时,在sn74lvc8t245通电时,会将A/B通道彼此隔离(Hi-Z),但两个通道(A&B)上的输入电路仍将处于活动状态,会使其浮动到Vcc/2的值。试试在通道两边的IO端口上增加100KΩ的下拉电阻。

  • 那如果把OE是能置低打开呢。两端连通,实测耗电也是18mA左右。那就是说不管八通道是否使用,全都初始加下拉电阻?20uA是在如下所示。

  • 原来您使用的是SN74LVC8T245-Q1,SN74LVC8T245与SN74LVC8T245-Q1参数是不一样的,我在SN74LVC8T245-Q1 datasheet上找到了上面表格。
    18mA左右您是Vcca =3.3V, Vccb = 5v, DIR 连接 Vcca, OE 连接 GND,测的ICCB吗
    加下拉电阻后,您可以实测一下ICCB电流是否可以降低。
  • 不好意思,我这边重新测试验证发现目前ICCB=18mA的条件是Vcca =3.3V, Vccb = 5v, DIR 连接 Vcca, OE 连接 Vcca。若把OE接地使能,ICCB降低至uA级别。那请问
    1.OE为高,A/B通道阻隔,ICCB电流大,仍然是因为输入电路仍将处于活动状态,会使其浮动到Vcc/2的值?我实测B通道信号都是低电平。请问内部接口电路是什么样子的呢?下拉电阻正在尝试飞线中。
    2.请问SN74LVC8T245-Q1与SN74LVC8T245两者主要的区别是?
  • 1、接口输入电路可参考下面文档:
    www.ti.com/.../scba004d.pdf
    2、TI芯片后缀带有Q1表示符合汽车应力测试合格标准AEC-Q100且适合在汽车应用中使用的设备上。带有“Q1”后缀的TI产品表明它们有资格用于汽车应用。如果不是汽车应用,可以使用不带后缀Q1的芯片。
  • 好的,谢谢