This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8020B CUP无法识别HUB设备,请帮忙检查下原理图是否正确?

Other Parts Discussed in Thread: TUSB8020BEVM, TUSB8020B

原理图如下:

  • 您好,

    原理图可以参考TUSB8020BEVM :
    www.ti.com/.../sllu196.pdf
  • 您好,电路没看出什么问题,晶振能正常起振吗?

    是否有按照datasheet上的 上电时序上电?

  • 晶振正常起振,GRSTz按照参考设计直接接1uF电容接地,VDD由VDD33通过DCDC转化的,时序按照datasheet上的来的,与参考设计不同的是 ,我的上端口接的是CPU,所以VBUS_DETECT直接是由1.1V通过两个10K分压的。还有就是上行和下行的USB2.0都没有接,直接悬空,这样会有影响么?I2C上挂了其他设备,是用的I2C功能,TUSB8020B是用的SMBUS这个功能这会影响么?
  • 看了参考设计,其他外围都跟参考设计相同,不同的是,我们使用TUSB8020B 去分CPU的USB3.0端口,一分为二,其中一路USB3.0是去了TypeC座子,USB2.0越过了HUB芯片,直接去了TypeC的座子。HUB上,USB2.0的脚全部悬空了。
  • USB2.0的引脚不用可直接悬空,没有影响。
    VBUS_DETECT这个引脚 建议的是使用90.9Kohm和10K的电阻分压,建议改下看是否能解决问题。
    I2C和SMbus 都可以。
  • 用90.9K和10K 去分过5V的,现象没什么变化,这个是检测的 ,只要给个合适的电平就行吧?因为我们的上行口是CPU,所以就用了供电的1.1V去分压的,所以是两个10K。
x 出现错误。请重试或与管理员联系。