This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

串行器DS90UB960的输入FPD-LINK的PCB走线的阻抗控制!



现在使用串行器DS90UB960的FPD-LINK接口通过连接器和同轴电缆连接相机,同轴电缆和连接器特性阻抗都为50欧,但是在我的PCB板的一段传输线特性阻抗计算出来只有40欧,和DS90UB960芯片手册上要求的50欧有不小的误差,请问这种情况下,对图像质量或显示有多大影响?会不会有致命影响到不工作,无图像?

  • 您好,
    同轴电缆和连接器特性阻抗都为50欧,PCB板传输线特性阻抗40欧,阻抗不连续,很容易将信号反射回去。一般将精度控制在10%,现在误差20%,再加上制版工艺误差,很难保证正常工作。
    建议PCB板传输线阻抗控制给制版厂家来做,让板厂给你调整参数,一般都与板材、加工工艺等有关。
  • 阻抗不连续会产生信号反射,会产生更多的噪声,信噪比会下降,信号完整性不能得到保证,对信号质量会有影响。看下数据手册推荐的最小阻值为45ohm。 所以传输线的特征阻抗不建议小于这个值,以免后续出现问题。

  • 是的,阻抗不连续对信号完整性有影响,只是当时做PCB设计时没考虑到这方面要求,现在PCB已经加工了,不能改了,计算阻抗有40欧,目前电路板还没调试,我就想知道阻抗为40欧这种情况对信号影响有多大?是不是很致命的,导致芯片不工作,接收不到图像?还是说有图像,只是图像质量不好?
  • 您好,阻抗40ohm的话误差有点儿大,datasheet推荐的能正常工作的特征阻抗为45ohm。 40ohm的结果不敢确定,因为没有这个实际数据可以参考,我个人的经验是能芯片能工作,并且应该也有图像,但是图像质量肯定不好。