您好,
本项目设计上需要用FPGA(XILINX SPATAN6)同时对5片LMX2595进行SPI配置,由于5片的配置参数一样,减少FPGA引脚使用,仅利用FPGA的三个引脚分别接到5片LMX2595对应的引脚处(SLK, SDI, CSB),FPGA引脚最大的输出电流是10mA左右,请问这种1根线驱动5路的方式是否可行,如果不可行,是否有对应的1分多的驱动芯片来满足这样的设计,非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
本项目设计上需要用FPGA(XILINX SPATAN6)同时对5片LMX2595进行SPI配置,由于5片的配置参数一样,减少FPGA引脚使用,仅利用FPGA的三个引脚分别接到5片LMX2595对应的引脚处(SLK, SDI, CSB),FPGA引脚最大的输出电流是10mA左右,请问这种1根线驱动5路的方式是否可行,如果不可行,是否有对应的1分多的驱动芯片来满足这样的设计,非常感谢
您好,我个人理解,除了考虑电流使能否驱动,还要考虑这种1分多,是否阻抗匹配, 如果阻抗不匹配,会造成信号反射。