This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD40106BM的输入阻抗是多少?

Other Parts Discussed in Thread: CD40106B

请问哪位大神知道CD40106BM的输入阻抗是多少?或者是从手册哪里可以看出来?

  • 逻辑器件的输入阻抗我们可以通过Vcc/Ileakage 计算得到。
    比如25度的时候,CD40106B的input current 为100nA 在18V的时候,那么常温下输入阻抗大约为180Mohm。
    事实上,CMOS输入的输入阻抗都比较高。
    Maximum Input Current Of 1 µA at 18 V Over Full
    Package Temperature Range:
    – 100 nA at 18 V and 25°C
  • 阻抗;可以看成电阻和电感/电容的组合,电阻是耗能元件分量,称为实部。电感/电容是储能元件分量,称为虚部。

    所以;对于输入阻抗,可以分解成电阻性泄漏和对地电容两个指标。

    对于绝缘性输入:

    由于电阻是非线性的,所以;定义绝缘电阻漏电流范围;为0.00001~0.1uA/25度

    输入电容为:5~7.5pF

    它们在数据表第5~8页。