This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有些产品上的CAN总线说是24V,我们的CAN总线是5V,现在需要两边的CAN能正常通讯,请问有什么的方案,或者CAN芯片模块?有没有电平是24V的CAN总线相关资料介绍?
接收端的输入共模电压范围+-12V指的是CANH或CANL端的电压范围。
我上面指的bus fault voltage +-58V指的是CANH或CANL能够承受的最大电压范围。
关于24V总线上的隐性或显性电平,还是要根据实际芯片的datasheet来看。
比如TCAN1044 这款,在不同负载条件下的隐性和显性电平范围是不一样的