This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962解串器能否接2个不同串化器,一个DS90UB953,一个DS90UB933?

我们有不同摄像头模组,一个是SENSOR接DS90UB933,信号是DVP;一个SENDOR接DS90UB953,信号是MIPI,这两个串化器能不能同时输出信号给DS90UB962来进行处理?

  • 您好,是不允许的, 962 的datasheet中有对多个输入源输入的要求, 一个是MIPI,一个是DVP,是无法做到输入同步的,

    Requirements:

    • Video arriving at input ports should be synchronized within approximately 1 video line period

    • All enabled ports should have valid, synchronized video

    • Each port must have identical video parameters, including number and size of video lines, presence of synchronization packets, and so forth.