实验中用到PCA9306芯片,想控制IIC电平1.8V到3.3V之间的转变。
Vref1直接连1.8V,Vref2和EN短接后通过200K电阻上拉到3.3V(这个和数据手册上要求一致);
scl1、sda1通过2.2k上拉到1.8V;
scl2、sda2通过4.7k上拉到3.3V;
我遇到的问题是:在没有任何IIC操作的情况下,scl1有1.8v,而sda1只有0.6V左右,scl2和sda2都在3.3V;Vref2和EN上的电压只有0.2V左右(感觉Vref2在内部被拉低了),请问这种问题一般是由什么引起的呢?希望大家多多指点,谢谢!