This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200 DDR3配置,关于SLP_S3信号的疑问?

Other Parts Discussed in Thread: TPS51200

Dear TI,

          目前正打算用贵司的TPS51200进行DDR3的VTT0.75V的配置,通过规格书的阅读发现,EN管脚,有的是直接接VCC3.3V,有的则是接的SLP_S3信号,请问有什么区别?如果接的是SLP_S3信号,这个信号是什么信号,来源于哪里,请帮忙解答,谢谢!

  • 您好,我看了下datasheet,EN接到SLP_S3 是专门在DDR VTT 应用上时,需要EN接在 SLP_S3上。
    在其他应用上, EN用来on/off 控制。
    SLP_S3 这个引脚我理解的是suspend的S3状态,SLP_S3 中的SLP我理解的是sleep, 因为休眠分为好几种状态,其中S3 为suspend。

    另外,TPS51200 是一款power的芯片,您也可以到“电源管理”版块咨询下我们的电源工程师。