Other Parts Discussed in Thread: TFP410
你好,我想请问一下,TPF410的I2C是与HDMI相连接的,与MCU未连接的时候,不通过I2C进行配置,要怎么样设置相应的引脚参数呢?原理图见附件lvds convert hdmi_v01_20191206.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TFP410
你好,我想请问一下,TPF410的I2C是与HDMI相连接的,与MCU未连接的时候,不通过I2C进行配置,要怎么样设置相应的引脚参数呢?原理图见附件lvds convert hdmi_v01_20191206.pdf
那么请问一下
1.我的数据进来之后怎么进行解析成HDMI信号呢?
2.I2C在这里需要连接到MCU吗?
3.MCU需要对芯片TFP410进行配置吗?
4.如果我不使用I2C,怎么对TFP410配置能达到把RGB888转化为HDMI信号?
谢谢
1. TFP410内部集成了TMDS encoder, 您可以参考7.2的应用框图,其中TMDS transmitter部分集成了TMDS encoder是用来将RGB信号编码为T.M.D.S信号的。
另外 7.3.1 T.M.D.S. Pixel Data and Control Signal Encoding 部分也有相应的介绍:
2. 如果不使能I2C的话,可以无需接到MCU上。
3.不使用I2C 芯片也是可以工作的,如果MCU端能够提供DE 信号的话,便可以不使用I2C。 如果MCU 不能提供DE信号,那么需要通过I2C 配置,TFP410 内部会产生DE信号。
4. 不使用I2C,也是可以实现RGB到TMDS 信号转换的。