This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn65dsi84 mipi转lvds驱动BOE32寸屏概率花屏的问题

Other Parts Discussed in Thread: SN65DSI84

方案:高通平台mipi转双8位lvds 

现象:开机概率花屏,见附件。

现象验证:

1、mipi信号不动,不断复位初始化sn65,概率出现花屏。同样花屏的时候再复位初始化sn65,大概率可以恢复正常。->mipi未动,问题不在于mipi数据。

2、花屏时拔掉lvds线,使得屏完全断电,再插上lvds线,仍然花屏。->屏已重启状态已恢复,lvds信号不符合屏。

3、花屏时,拔出lvds线,插入另一个型号屏的lvds线,显示正常。再插回原屏,仍然花屏。->与屏有相关,lvds信号不符合此屏,但是符合另一个型号屏。

请帮忙分析原因,十分感谢。DV320FHM-NN0 Product Specification_RewO.pdf

  • 您好,首先您的显示屏接收的LVDS 电压swing范围为+-100mV~+-300mV。sn65dsi84的LVDS输出swing电压是通过0X19这个寄存器来控制的,相应的Vod范围以及配置参考Page9的Electrical Characteristics 部分介绍,使得SN65DSI84输出LVDS电压范围要满足显示屏的输入电压范围才行。
    其次就是我看了下附件中显示屏,并没有内置100ohm 匹配电阻,那么就需要在靠近屏的LVDS端需要端接100ohm匹配电阻。 请验证下是否还花屏。
  • 1、屏规格书上在page9上提到Note3:The LVDS test point is at each terminal resistor。但是没有注明阻值。
    2、实际测量近屏LVDS端的阻值为112ohm,但是有其中一个LVDS_B_Y0通道的阻值为105ohm。
    3、寄存器0x19目前为0x00,曾经调到过0x0f,并没有效果。
    请问,就适配这款屏,阻值并不是标准的100或200欧,寄存器0x19应如何配置?
  • 寄存器0x19设为0x05和0x0a,都没有效果。
  • 补充信息:花屏现象出现后LVDS12V出现下拉的干扰波形,拔出LVDS线,干扰波形消除。再插回,花屏现象和干扰波形仍在。

    似乎是不符合屏要求的LVDS信号导致屏工作异常了。

  • 你好,问一下你dsi的mode_flags是怎么设置的?感谢
  • dsi的mode_flags是什么参数?Qualcomm没有找到同名的参数。

    有traffic-mode这个参数。
    qcom,mdss-dsi-traffic-mode = "burst_mode";