Hi
TUSB8041 EVM上,TUSB8041是通过USB3 TYPE B连接到host端的,芯片的SSTX引脚接了AC耦合电容。
现在我把TUSB8041直接放到板子上,与host相连,那么是否SSTX和SSRX信号上都需要接AC耦合电容呢?如果是,电容靠近哪端放置呢?PS:主板采用核心板+底板的方式,核心板与底板通过板对板连接器连接,TUSB8041放置在底板上。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TUSB8041 EVM上,TUSB8041是通过USB3 TYPE B连接到host端的,芯片的SSTX引脚接了AC耦合电容。
现在我把TUSB8041直接放到板子上,与host相连,那么是否SSTX和SSRX信号上都需要接AC耦合电容呢?如果是,电容靠近哪端放置呢?PS:主板采用核心板+底板的方式,核心板与底板通过板对板连接器连接,TUSB8041放置在底板上。
可能我没说清楚,我这边的应用是把CPU与TUSB8041直接连接的,中间没有USB连接器或线缆,这种情况下,是否只在SSTXP/SSTXN上加AC耦合电容就可以了?
另外,TUSB8041的55/56引脚是输出(SSTXP/SSTXN),应连接到CPU的SSRXP/SSRXN上,对吧,那为什么参考里,这组线上要加耦合电容呢?如果这里加了电容,那CPU的SSTXP/SSTXN到TUSB8041的SSRXP/SSRXN之间是否也应该加电容呢?