使用两块TI官方LMX8410评估板,OSCin 50MHz,LO 4860MHz,RFin 4800MHz,IFout 60MHz,SYNC为10MHz非连续脉冲信号,其中OSCin和RFin以及SYNC均为同步,外部手动触发SYNC脉冲信号,一直无法进行相位同步,请教一下实现相位同步的具体步骤是什么样的呢?感谢!
备注:OSCin和SYNC均为外部HMC7044提供的同步信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1 首先针对您所提到的第1项,参考datasheet,规定最小应该为1.4V,这里是否理解正确?
现在我的SYNC电平如波形图所示:
如图所示,SYNC上升沿距离OSCin上升沿至少大于3ns,这一点应该满足,其次,高电平持续时间达到us级别,应该也满足tHOLD,关于您所提到的tSETUP,无法理解,可否详细说明一下呢?
---------------------------------------------------------------------------------------------------------
2 SYNC信号幅值如下图图所示,0V-1.4V似乎刚好满足,接近临界点,这里是否是因为SYNC信号幅度不够从而导致有时候无法识别SYNC信号,无法同步呢?
---------------------------------------------------------------------------------------------------------
3 SYNC信号波形如下图所示:
红色波形为OSCin,蓝色为SYNC脉冲,观察SYNC信号可知,在脉冲信号前方和后方均产生一个约950mv的毛刺,这是否会使8410误辨别为SYNC脉冲从而产生错误同步呢?
---------------------------------------------------------------------------------------------------------
希望能得到您的解答!非常感谢
祝好!