This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

加解中芯片947和948的mode配置



在用947和948的芯片时遇到一个问题,目前947的mode1的硬件配置为47K下拉,按文档中的说明,应该是OpenLDI的mapping,

但是寄存器中的描述不确定是不是反的,1对应的是OpenLDI的配置,

  • 您好, 没有反,是两种配置openLDI的方式,一种是通过strap pin MAPSEL=0的方式,一种是通过寄存器配置,0X4F 的bit7=1 的方式.
    通过这两种方式中的任意一种都可以配置为openLDI的data mapping方式.
  • 我硬件上将947的mode1配置成下拉,即接47K下拉电阻,那上电启动后应该就是OpenLDI的模式,但是寄存器读出来4f的bit7是0,不是1,所以想确认下,是不是规格书写反了。

  • 您好,感谢您的反馈,寄存器0X4F bit7是写反了,应该是0 时为OpenLDI mapping,1时为SPWG mapping。
    另外还有一处也是反的,不过这点在Table8的下面备注note中有给出。就是0X4F 的bit6 OLDI_IN_MODE 也是写反了。
  • Kailyn,哪现在还有一个问题,我主芯片这边配的是spwg 的mapping,947硬件配置的是openldi,948硬件配置为MAPSEL= H,屏这边为vesa格式,按这样的配置,显示是错误的,需要将以上四个的配置任何一个换成另一种才能正常显示,主芯片和屏这边的配置我确认是正确的,请帮忙确认下你们947和948中关于上电默认配置是否正确,谢谢。以下截图分别为947,948及屏的格式选择。