Hi
我用TUSB8041设计了一个hub,原理图如下,请帮忙评审下原理是否有问题,谢谢!TUSB8041原理图.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
我用TUSB8041设计了一个hub,原理图如下,请帮忙评审下原理是否有问题,谢谢!TUSB8041原理图.pdf
您好,
建议您参考数据手册9.2.1.2 Detailed Design Procedure部分。
也有TUSB8041EVM参考:www.ti.com.cn/.../TUSB8041EVM
请注意:USB上行接口,在TX信号线上串接的0.1uF电容,放在USB HUB板上,在RX信号线上串接的0.1uF电容,放在USB host板上,即都放在TX端。
目前在另外一块板卡上面正在调试这款芯片,50引脚空焊,给TUSB8041芯片的3.3V先上电1.1V后上电,结果CPU不能够正常识别TUSB8041芯片,将50引脚对地短接一下CPU有时候能够识别TUSB8041芯片。先提出以下两点问题:
关于上电时序问题:
1、3.3V跟1.1V上电顺序是什么
2、50引脚接电容的话对上电时序有什么影响