Other Parts Discussed in Thread: MSP430F149
如何进入SN65HVD3082的shutdown mode,我按照数据手册的使用方法,“When both the driver and receiver are disabled (DE low and RE high) the device is in shutdown mode.”可是无法进入到shutdown mode。
你好,感谢你的回答,你说的这个"但DE为low,RE为high的时间不低于60ns“,具体意思不清楚,我就是用两个IO口控制使RE置高,DE拉低。我贴上的用到shutdown的一段代码,使用的MSP430F149,需要进入到LPM3,在进入到LPM3之前使sn65hvd3082进入到shutdown模式,这段代码有错误吗?
__disable_interrupt(); //防止IO口误触发中断。
PC_DROUT |=PC_DR; //RE置高
PC_TROUT &=~PC_TR; //DE拉低 rs485芯片置为standby mode
P1IES |= POWER; //下降沿产生中断
P1IE |= POWER; //P1.4IO口中断使能
P1IFG =0x00; //软件清除中断标志位
ClearLCD();
if(g_ucLowPowerFlag == 1)
{
LCDStringDisp(CenterFunction("电压过低 "),2,"电压过低 ",0);
LCDStringDisp(CenterFunction("请充电 "),4,"请充电 ",0);
}
delay_ms(100);
__enable_interrupt();
_BIS_SR(LPM3_bits + GIE); // Enter LPM3