This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

以太网DP83848I刚开始可以使用,但是DP83848I芯片调试使用一两周后陆续出现永久无法连接到网络的问题,把以太网芯片取下来换了新的DP83848I芯片又可以使用了

Other Parts Discussed in Thread: DP83848I, TPS23758

以太网DP83848I芯片调试一两周后出现无法连接交换机/路由器,STM32访问DP83848I 初始化能够通过,但不能分配动态IP地址,不断触发检测网线插拔的函数,出现以太网连接断开连接断开的问题,就好像网线被拔了断开拔了断开的现象,然后换了同一批新的DP83848芯片,就可以成功连接通讯了,初步怀疑是芯片被损坏, 现无法定位问题所在,板子采用的是POE方案TPS23758隔离式输出5V经过LDO稳压到3.3给DP83848芯片供电,请TI的大佬帮忙指导分析  十分感谢。

DP83848原理图:

RJ-45网口插座内部图

 

采用POE方式进行供电,PD受电芯片TPS23758原理图部分如下,插上网线后可正常供电,输出5V电压。

 

测量没有出现问题的以太网DP83848I的TX管脚的电压波形如下:

 

测量有问题的以太网DP83848I的TX管脚的电压波形如下:

 

  • 以太网DP83848I芯片调试一两周后出现无法连接交换机/路由器,STM32访问DP83848I 初始化能够通过,但不能分配动态IP地址,不断触发检测网线插拔的函数,出现以太网连接断开连接断开的问题,就好像网线被拔了断开拔了断开的现象,然后换了同一批新的DP83848芯片,就可以成功连接通讯了,初步怀疑是芯片被损坏, 现无法定位问题所在,板子采用的是POE方案TPS23758隔离式输出5V经过LDO稳压到3.3给DP83848芯片供电,请TI的大佬帮忙指导分析  十分感谢。

    DP83848原理图:

    RJ-45网口插座内部图

    采用POE方式进行供电,PD受电芯片TPS23758原理图部分如下,插上网线后可正常供电,输出5V电压

    测量没有出现问题的以太网DP83848I的TX管脚的电压波形如下:

    测量有问题的以太网DP83848I的TX管脚的电压波形如下:

  • 由于电压的供电来源采用的是TPS23758变压器隔离反激式方式,板子上面RJ-45网口插座的屏蔽壳接的是DP83848的地,不是POE输入的地,不知道是否是导致问题的关键。
  • 由于电压的供电来源采用的是TPS23758变压器隔离反激式方式,板子上面RJ-45网口插座的屏蔽壳接的是DP83848的地,不是POE输入的地,不知道是否是导致问题的关键。
  • 您好,
    图片都没有显示,请点击回复对话框右下角蓝色字体“使用高级编辑器编辑文本”,上传图片,谢谢!