This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84ZQER接口问题

哈喽:TI

我们有个项目使用SN65DSI84ZQER,mipi转换LVDS,1920*1080分辨率,请问一下输出信号需要接两组吗?一组输出支持最大多少分辨率

  • 您好,
    感谢您对TI产品的关注!为更加有效地解决您的问题,我需要多一些时间查看这款芯片,再为您解答。
  • 您好,输出LVDS 可以是single link也可以是dual link,每个link都是包含4对data+1对clock。所以只用一组是可以的,另外一组可以直接悬空。
    LVDS clock的频率范围为25Mhz~154Mhz,如果您是1920*1080p@60hz的分辨率的话,需要的像素时钟频率为148.5MHz. 这个是根据水平和垂直的有效像素计算得到的,如果水平和垂直总的像素计算的话,考虑到像素的blanking,1920*1080p@60hz 的分辨率需要的LVDS clock为153.6Mhz。所以DSI84 的LVDS 像素时钟最大能支持到154MHz,是能够支持1920*1080p@60hz的分辨率。
  • 您好,可查看下面手册的第7个FAQ:
    www.ti.com/.../slla356.pdf