This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】如何端接LVDS

Other Parts Discussed in Thread: DS90LV028A, DS90LV048A, DS90LV011A, DS90LT012A, DS90LV047A, SN65LVDT34, DS90LV012A, DS90LV027A, SN65LVDS348, SN65LVDS352, SN65LVDS34, SN65LVDS33, SN65MLVD204B, SN65MLVD040, SN65MLVD206B, SN65MLVD205A, SN65MLVD207

本文档讨论了具有DC和AC耦合配置的LVDS驱动和接收器的端接和偏置方案。它还显示多支路和多点(M-LVDS)连接的端接方案。

直流耦合配置

将诸如DS90LV011A、DS90LV027A或DS90LV047A等LVDS驱动连接到诸如DS90LV012A、DS90LV028A或DS90LV048A等LVDS接收器极其简单,仅需在接收器的输入端对上跨接一个100差分端接电阻即可,如图1所示。该端接电阻应尽可能靠近接收器放置,以在接收器输入端产生差分电压,并匹配传输线阻抗以减少反射。某些LVDS接收器诸如DS90LT012A、SN65LVDT34或SN65LVDT32等内部已经集成了100Ω端接电阻。使用此类接收器时,外部则不再需要端接100ohm匹配电阻。

另一种端接方案如图2所示。它使用两个电阻分流端接,并且中间使用一个电容到地的端接方法。该电容器可滤除共模噪声并有助于抑制传输线产生偏差(这可能是由于差分线不匹配或驱动输出产生偏差)。电容器的值取决于工作频率,就像把它看作交流分量短路。0.1 µF的电容值对于大多数高数据速率(1 Mbps及更高)已足够。


交流耦合配置

图3所示为交流耦合配置下的端接。请注意:对于交流耦合,需要对传输的数据进行直流平衡(例如,使用8b/10b编码)。图3中,接收器输入端的电阻网络将DC共模恢复到1.2 V(假设Vcc = 3.3 V),这处在标准LVDS接收器的输入共模范围的中间值。此外,电阻器网络在接收器的输入端提供100Ω端接。如果在LVDS接收器中集成了端接电阻,则应选择更大的电阻值,以免改变接收器输入端的有效端接电阻。建议的上拉值为10kΩ,下拉值为5.7kΩ。交流耦合电容的值取决于工作频率,因为它隔离直流分量,但是看起来就像是交流分量短路。0.1 µF的电容值对于高数据速率(1 Mbps及更高)已足够。

图 4所示为另一种电路。该电路除偏置电阻网络外,还使用分流端接和中间加电容到地的方法。该电容器可滤除共模噪声并有助于减少传输线偏差。与图3中的电路相比,该电路的另一个优点是功耗更低。

图5所示为图3中电路的另一种变型。其仅使用一对电阻在负输入端子上提供偏置。正输入端子还将通过100-Ω端接获得共模电压。这种方法的优点是减少了零器件的数量。缺点是正负输入端之间存在一定的偏差。

 

当使用诸如SN65LVDS33、SN65LVDS34、SN65LVDS348和SN65LVDS352等具有宽共模范围的LVDS接收器(输入共模范围为–4V至5V)时,则无需共模偏置电阻器网络。如图6所示,仅需要100Ω端接.

 

多支路LVDS端接

在多支路配置中使用LVDS收发器时,仅需要在最远接收器的输入端上端接100ohm匹配电阻,如图7所示。

在半双工多点配置中使用诸如 SN65MLVD206B、SN65MLVD204B或SN65MLVD040等M-LVDS收发器时,需要在总线两端进行端接,如图8所示。不必将端接置于靠近接收器的位置,而是将其置于总线两端的最远点。

如果使用诸如SN65MLVD205A或SN65MLVD207等全双工M-LVDS收发器,则使用两个差分对,每个差分对在连接两端都需要两个端接,如图9所示。

x 出现错误。请重试或与管理员联系。