This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】浅谈RS485的单位负载

Other Parts Discussed in Thread: THVD1500, THVD1450, THVD1429

我们经常在RS485 transceiver的datasheet中看到类似这样一句话:

1/4 Unit Load Allows for 128 Devices Connected on Bus(SN75LBC184.pdf

这句话的意思是,1/4单位负载,允许总线上挂接128个节点。那么什么是单位负载(unit load)呢?简单来介绍下:

一条485总线上节点数量的限制条件是:有源驱动器的总电流负载。我们是用单位负载来衡量RS485总线驱动能力的,单位负载的定义则是根据标准的485总线接收器的输入阻抗(12Kohm)来定义的,标准的RS485总线能够驱动32个单位负载(即32个12Kohm并联)换句话说,485总线负载电阻Rload不能大于375欧姆。一些485接收器的输入阻抗为48Kohm(1/4 unit load)或者是96Kohm(1/8 unit load),那么相应的总线可挂接的节点数分别为128个和256个。另外,不同输入阻抗的485接收器可以连接在一起,只要保证并联输入阻抗不能超过32个单位负载(即总线负载Rload<=375Ohm)

 

目前TI的收发器能够挂接的节点数为256个的系列有:THVD1500 /1510/1550

 

另外,需要提及的就是,RS485的应用环境比较复杂,接口一般需要满足ESD, EFT, Surge的规范要求, 所以我们在设计外围电路的时候接口通常需要加上TVS做保护,而TI的收发器本身都集成了ESD防护,比如THVD1450这款具有±18-kV IEC ESD protection,并且和以往的收发器相比,它有着比较宽范围的差分输出电压,从而更好的抑制噪声。

 

如果实际应用中需要承受更高电压或电流浪涌的话,可以选择THVD1429这款,和THVD1450有着相似的电气特性,但是HVD1429还集成了Transient和surge保护。

x 出现错误。请重试或与管理员联系。