Other Parts Discussed in Thread: CDCM9102, CDCE62002, CDCM6208, TMS320C6678
CDCM9102输出时钟为LVPECL电平时,VOH min(2.12)略小于C6678输入接口LVPECL电平的VIH min(2.135)
请问这样可以直接使用吗?
如果使用CDCE62002的话,应该是可以直连的。
但CDCM9102是PCIe专用的,比较纠结这两个芯片应该用哪个
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CDCM9102, CDCE62002, CDCM6208, TMS320C6678
CDCM9102输出时钟为LVPECL电平时,VOH min(2.12)略小于C6678输入接口LVPECL电平的VIH min(2.135)
请问这样可以直接使用吗?
如果使用CDCE62002的话,应该是可以直连的。
但CDCM9102是PCIe专用的,比较纠结这两个芯片应该用哪个
您好,两个接口之间如果可以直接连接,要满足以下两个条件:
1)driver的输出Voh(min)要大于receiver的Vih(min)。
2)driver的输出Vol(max)要小于receiver的Vil(max)。
所以严格意义来讲,是不可以直接使用的。