This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948 应用

你好,我想设置948一路RIN两路oldi模式。

1.输入是自动识别吗mode_sel0 设置no.4  mode_sel1no.1还是no.3怎么选。

2.high-speed back channel干嘛用的

3.tft的clk  20-110mhz,这种1to2是否支持

  • 您好,感谢您对TI产品的关注!为更加有效地解决您的问题,我需要多一些时间查看这款芯片,再为您解答。
  • 您好,1、默认情况下,FPD Link III接收器根据1或2-lane模式操作自动配置输入,对寄存器0x34[4:3]设置将覆盖自动检测。
    2、back channel用于传输低带宽数据,如I2C、控制和GPO信号,参考数据手册7.3.2和7.3.9.2 部分说明。
    3、在1-Lane FPD-Link III Input, Dual Link OpenLDI Output模式中,PCLK速率可以从50Mhz到96MHz,tft的clk 最小为20MHZ是支持的。
  • 你好,我现在有个产品,948,采用两路port输入可以正常显示,但去掉port1的外围电路,芯片引脚悬空。产品就无法显示了,只有背光,是什么情况,其他都没变