This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941展频

我们现在有个应用方案是soc -》DS90UB941-->DS90UB948-->LCD,我们看到941规格书上支持SSC输入,但是948上面没有说SSC功能,那么我们现在如果SOC输出展频的DSI信号到串行器941,然后948进行解串出LVDS信号也会被展频吗?还是948按固定频率输出LVDS信号?

  • 您好,SSC是对基波,或者高次谐波的峰值有抑制作用,或者说能够有效的抑制EMC。
    UB941 支持SSC功能,也就是说能够有效的抑制Soc 输出时钟频率的EMC作用。 我理解的是948 解串出的lVDS信号不会被展频,是按固定频率输出的LVDS信号。
  • 另外想咨询UB947规格书中没有写支持SSC功能,如果soc侧输出的LVDS时钟是带展频,那UB947是不是会存在就收LVDS信号出错的情况

  • 您好,UB947不支持SSC 的话,就不建议Soc端输出带SSC的时钟信号给947.