This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954与 933的配置,不出图!,求解



OV9706+OV496+DS90UB933+ DS90UB954 ,接934能直接点亮,用954不能点亮

(1)其中地址:

OV496:0x48

933:0xb0

954:0x68

(2)RX0输入,mipi  4lane输出  ,,1280*720@25fps, lock,pass均显示高电平

配置文件如下:【地址】【寄存器】【值】【8地址8数据】

0x68,0x33,0x01,0x0808

0x68,0x20,0x00,0x0808

0x68,0x4c,0x01,0x0808
0x68,0x6d,0x7f,0x0808
0x68,0x7c,0xc1,0x0808
0x68,0x58,0x58,0x0808
0x68,0x5c,0xb0,0x0808
0x68,0x5d,0x48,0x0808
0x68,0x65,0x48,0x0808
0x68,0x72,0xE8,0x0808
0x00,0x00,0xff,0x0808
0xb0,0x0d,0x99,0x0808

测量到有mipi信号,,但是不出图,,,,求解怎么个问题

  • RAW12转YUV422 8bit输出

  • 您好,UB954 如果配置为YUV422的话,需要配置寄存器0X70=0X1E. 您检查下是否这个寄存器配置问题导致没有输出?
  • 1)经确认,ISP到933,只用到DIN2~DIN9    8位,故是RAW10的8bit传输转 YUV422  8bit,,所以0x70 设置0x1e

    (2)0x7C,的【7:6】选择10模式的高8bit,这点我的理解是否正确? 而极性确认,FV为0有效,LV为1有效。。。故设置0x7c:0x81

    (3)有个疑问就是我搜索I2C设备地址,只搜到954地址0x68,搜不到933或496(ISP)地址,,只有配置了以下寄存器,才会显示分配的地址,那么想知道,分配出的地址是否应该设置跟我硬件电路的地址一致呢???我硬件496地址 0x48,933地址(7bit)0x58,(8bit write为0xb0)

    (4)sensor为外同步模式,这里所说的同步是否为帧同步信号?如果是,我这边sensor已经设置为不需要帧同步,所以这个0x21是该怎么配置呢

     

    更新后的配置如下,有信号,但还是不出图

     

    0x68,0x33,0x01,0x0808   // CSI-OUT 使能

    0x68,0x20,0x20,0x0808  //禁RX-PORT1,使能RX-PORT0传递

    0x68,0x4c,0x01,0x0808  //使能写 RX PORT0

    0x68,0x6d,0x7f,0x0808  // FPD III输入模式-RAW10/100MHZ

    0x68,0x7c,0x81,0x0808  //高8位处理(Y9~Y2),极性 行-0,场-1   [7:6] 11? 10?

    0x68,0x58,0x58,0x0808  //I2C透传使能,反向通道使能,2.5Mbps

    0x68,0x5c,0xb0,0x0808   //7位远程serdes别名ID

    0x68,0x5d,0x48,0x0808  //7位远程从地址 48 (ISP电路地址一致)?

    0x68,0x65,0x48,0x0808  //7位远程从地址 48  ??(为何与0x5d要重复设置)

    0x68,0x70,0x1e,0x0808  // RAW10  8bit

    0x00,0x00,0xff,0x0808 

    0xb0,0x0d,0x99,0x0808  //933的GPIO0,GPIO1均使能置高

  • 你出图了么,能分享下配置么?