This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104EPWR串口电平转换问题

你好,使用TXS0104芯片串口通信电平1.8V转5V电平,软件TX端一直发送数据,发现上电的时候刚开始可以采集到串口信号,过一会瞬间就没有信号了,输入端一直1.8V高电平,输出端一直是5V高电平,就是没有数据输出。不焊接TXS0104芯片,1.8V串口数据信号一直都有,请问是怎么回事?

  • 您好,您的意思是当TXS0104 上电瞬间,1.8V信号是有的,过一段时间,输入端的1.8V信号也没有了是吗? 还是说输入信号一直有,但是输出没有信号?我看您是将OE信号一直上拉的, 建议在上电瞬间, OE拉低,当电压起来稳定之后,再将OE拉高试试呢? 

  • 问题找到了,A2通道UART_CTS一直被MCU拉低,导致输入信号一直高电平,输出也是高电平。断开A2通道,数据就正常了,请问是怎么回事,这几个通道不是独立的吗?

  • 您好,这几个通道确实是独立的,理论上通道之间是不会相互影响的。
    CTS信号是clear to send信号,低有效吗? 所以我认为要看下UART中CTS拉低对TX和RX的影响,不是TXS0104导致。
    本身TXS0104的每个通道其实是独立的。
x 出现错误。请重试或与管理员联系。