This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISX019+TI933,后端是TI960,做环视系统,TI933和TI960是否可以不配置

Camera端使用的是ISX019+TI933,1280*720,通过TI的GPIO1做外触发给FSYNC,后端使用是TI960,做环视系统。

以上搭配960和933是否可以不配置,摄像头那端就直接改为内触发。

  • 您好,关于您的这个问题,  是否需要配置寄存器,要看每个寄存器的功能您是否需要, 如果不需要这个功能,那么默认配置就可以.

    但是如果您需要这个功能,相应的也就需要配置这个寄存器.