This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947 输入信号是8组LVDS信号和一组时钟,如何对应前端芯片的8组LVDS信号和2组时钟输出,视频分辨率为1920*720,需要如何连接和设置?

请教如题的问题:

视频分辨率为1920*720, 前端视频处理芯片输出8组LVDS和2组时钟(D0-D3,CLK1, D0-D3,CLK2)此接口与DS90UB948输出接口是一样的,也与液晶屏接口是一致的,但是如何跟DS90UB947(D0-D7,CLK)对应连接和相关设置?因为947只有8组LVDS和1组时钟,谢谢!