Other Parts Discussed in Thread: TFP401A-EP, TFP401A
Hi
有几个问题请帮忙支持一下
1. 请问TFP401A-EP输入端是否可以直接连接HDMI的视频信号?
2. TFP401A-EP输出端是否可以接到FPGA内做信号处理?
3. 从哪里可以获得详细的TFP401A-EP的设计资料,包括寄存器配置,参考设计等。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TFP401A-EP, TFP401A
Hi
有几个问题请帮忙支持一下
1. 请问TFP401A-EP输入端是否可以直接连接HDMI的视频信号?
2. TFP401A-EP输出端是否可以接到FPGA内做信号处理?
3. 从哪里可以获得详细的TFP401A-EP的设计资料,包括寄存器配置,参考设计等。
您好, TFP 401A-EP 是TMDS receiver, 可以接收HDMI的TMDS信号,但是不包含音频信号.它的资料都在产品主页的technical documents里.

另外,后缀EP代表的是enhanced products产品, 主要用于航空航天等级, 如果是普通应用的话,可直接使用TFP401A, 不需要使用EP产品.
Dear Kailyn,
你看我是不是可以这样理解:
1. TFP401A-EP可以接收标准的HDMI(1920x1080)TMDS信号并解码成并行数据。
2. 可以将DATA0(Blue)TMDS信号中的行场同步时钟解码出来。
3. 无法将DATA1(Green)和DATA2(Red)TMDS信号中的左右音频数据解码。
请给予明确答复,非常感谢!
Dear Kailyn,
事实上,我的应用是只需解码出标准的HDMI信号的TMDS_D0信号,即解码出行、场时钟和Blue数据。对于HDMI的TMDS_D1和TMDS_D2数据我是不需要的,即不需要Green数据和Red数据。请不必猜测我是否需要audio信号,请直接回答我的问题,是或不是,行或不行即可。
1. TFP401A-EP可以接收标准的HDMI(1920x1080)TMDS信号并解码成并行数据。
2. 可以将DATA0(Blue)TMDS信号中的行场同步时钟解码出来。
3. 无法将DATA1(Green)和DATA2(Red)TMDS信号中的左右音频数据解码。
4. 我最关心的是对于标准的HDMI视频数据格式,该芯片能否正确解码TMDS_D0信号?
谢谢。