This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI934+TI935+OV2310

Hi

我这边使用TI934解串板设置寄存器如下

0x4c,0x01,

0x58,0x58,

0x5c,0x32,   //935 I2C地址

0x5d,0xC0,  //Sensor  I2C地址

0x65,0xC0,  //Sensor  I2C地址

 

对TI934写如上寄存器后不能找到TI935通讯地址,请问我还需要做哪些其它设置?

另外我这边也有TI954开发板,请帮忙参考两种解串板如何设置可以通讯TI935和Sensor OV2310?

  • 您好,您的这个问题和前几天一个客户的问题比较像, e2echina.ti.com/.../195229
    现在是host无法和remote serializer进行通讯,读取不到935的地址.
    和935通讯,serializer ID是自动加载到deserializer端的,另外还需要配置SER Alias ID.
    您先读取下自动加载到934中的935的ID是否能正确读取到? 从而确认link是否没问题呢.