This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953+DS90UB954+OV2740是否能够实现

TI的大神,你们好!

我想用OV2740+DS90UB953+DS90UB954组成一个摄像系统!

但是现在的问题是不知道DS90UB953能不能接受并正确解码OV2740的视频流,OV2740接口是MIPI CSI-2,视频格式是10bit RGB RAW;不知道DS90UB953能否与其匹配!

如果DS90UB953能够正确接受并成功将数据发送给DS90UB954,DS90UB954的MIPI CSI-2 接口输出的视频格式是否能够还原成OV2740输出的一样?
急急!请大神们解答一下!谢谢!

  • 您好, 关于数据格式的问题,我以前请教过美国工程师,他的回复是:For 953 to 954 everything is CSI-2 so whatever data type is sent to the 953 is passed unchanged through the 954. It can support an CSI-2 data format.
    所以我的理解是UB953 能接受任何CSI-2 的数据格式. 并且经过UB954之后能正确解码,恢复到以前的数据格式.