This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941搭配DS90UB948调试 10寸屏输出正常,12寸屏显示花屏

DS90UB941搭配DS90UB948调试 10寸屏输出正常,然后接12寸屏显示花屏,请问需要注意哪些地方的改动?

  • 您好,是一上电花屏,还是说电压起来稳定之后, 没有改善,仍然花屏? 花屏时,lock输出什么电平?
    建议参考datasheet中9.1 Power-Up Requirements and PDB Pin 部分的介绍以及Figure 55的上电时序,看上电时序是否正常? 先排除是否上电时序导致的花屏问题.
    www.ti.com/.../ds90ub948-q1.pd
  • 你好,检查过不是时序造成的,怀疑是和屏的分辨率配置有关,不知道941上有没有这一块的配置项

  • 如果和屏的分辨率配置有关,需要改变屏的参数,941上是无法修改分辨率的,它只是serializer,作用是对数据进行编码,只能说它能够支持多大的分辨率。
  • 如果和屏的分辨率配置有关,需要改变屏的参数,941上是无法修改分辨率的,它只是serializer,作用是对数据进行编码,只能说它能够支持多大的分辨率。
  • Hi Kailyn,我们现在的疑问就是不知道该修改什么。现在的情况是947-948,10寸,12寸屏都ok了,941-948,10寸屏ok,12寸屏不行了。那941上有没有哪些寄存器,看够解析出来,我前端发的数据的分辨率之类的,或者有没有其他可以读出相关的值判断问题。

  • 您好,941 您使用的是single link还是dual link?因为single link的话,941能够支持的像素时钟最大为105Mhz。
    941 接10寸的屏OK, 12寸的屏不行, 有没有看下屏的spec,10寸和12寸的参数上有什么区别?
  • 941用的single的,我们屏10吋的比12吋的分辨率高,10吋的1600*1200,12吋的1290*720
  • 1600*1200,60hz帧频吗?如果是1600*1200@60Hz的话,需要像素时钟频率162Mhz,single link的941 是不支持的,要么您是30Hz帧频。
    12寸的您这里写的应该是1920*720,这个分辨率低,假设60hz的话,计算下来105MHz应该是支持的。 所以排除是分辨率的问题导致。

    您能附上12寸屏显示的截图看下吗?