This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220 TX和RX对调问题

Other Parts Discussed in Thread: HD3SS3220

1.HD3SS3220 datasheet中的参考设计 USB3.0的 IC的TX差分对接到了HD3SS3220 TX端,IC的RX差分对接HD3SS3220 RX端;而EVM的参考设计IC的TX接HD3SS3220的RX,IC的RX接HD3SS3220的TX,这样是否矛盾,还是都兼容

2.EVM参考设计中CRX2P、CRX2N未做N/P交换,而CRX1N、CRX1P做了差分对内N/P交换,如果需要进行N/P交换,HD3SS3220输出端需要4组输出都做N/P交换,还是只有2组输出做N/P交换就可以

  • 您好,
    HD3S3220是无源开关,因此可以交换其TX&RX引脚,也可以交换差分对极性
  • HD3S3220是无源开关,交换TX/RX我理解了。但是输出端由两组TX1 RX1、TX2 RX2;EVM中只有TX1 RX1交换了极性而TX2 RX2没有交换极性

  • HD3S3220是无源开关,交换TX/RX我理解了。就是输出端TX RX交换了,那输出端TX RX也要交换。
    但是不理解:输出端有两组TX1 RX1、TX2 RX2;TX1 RX1差分对内P/N交换了, 而TX2 RX2 /N没有交换,会不会造成TYPE C端子正插入时逻辑0,反插入时变成逻辑1,因为TX1 RX1差分对内P/N交换了, 而TX2 RX2 P/N没有交换
  • 您好,USB 3.0 差分对的极性可以交换是由 USB 3.0 协议规范的,参考USB 3.0规范第6.4.2节