This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH949A调试

Other Parts Discussed in Thread: HD3SS215, DS90UH949A-Q1

你好,

我使用DS90UH949A设计了一个HDMI转FPD Link的串行器,请问在还没有解串器与显示屏的情况下如何进行调试。

谢谢

  • 您好,没有解串器的话,输入给HDMI源,可以在UH949输出端用示波器观察FPD link的波形。
    但是serializer 是要和deserializer 搭配一起使用的。
  • 你好,
    由于我采取HDMI输出和FPD-link复用的显示方式,因此使用HD3SS215——DS90UH949A-Q1作为FPD link串化路径,当HD3SS215选择FPD link输出时,DS90UH949A-Q1选择 IDx接地,MODE_SEL0接地,MODE_SEL1接地。在我的理解中这样会选择内部预编程的EDID,但是通过测量DDC信号发现DDC信号一直为高电平,请问可能时什么原因?
    谢谢
  • 你好,
    我希望可以在没有解串器和屏幕的情况下调试949,通过示波器测量HPD信号一直为低电平,请问这可能是什么问题导致的,有什么办法在解串器和屏幕的情况下将此信号拉高,单独调试949.
    谢谢
x 出现错误。请重试或与管理员联系。