This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

949 交流耦合与直流耦合问题

Ti 支持团队你好,

请问949电路中由VTERM Pin 设置的直流耦合与交流耦合对HDMI输入电路有什么要求吗?若对输入有要求,那么输入是直流耦合的,但是VTERM Pin接1.8V会对949芯片或HDMI源产生损伤吗?

  • 您好,AC耦合和DC耦合指的是HDMI信号,也就是说如果AC 耦合的话,耦合电容是加在靠近HDMI信号端的,即IN_CLK+— 和IN_Dx+/-这几对HDMI信号。 如果HDMI差分对是AC耦合,那么Vterm接的是1.8V,如果是DC 耦合的话,那么Vterm接的是3.3V。
    如果输入是DC耦合,那么Vterm需要接的是3.3v,否则会影响性能。