This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320IRWBR的ID管脚上拉4.7KΩ电阻到3.3V是否可以

TUSB320IRWBR的ID管脚在手册中建议上拉电阻200K,但是由于与其连接的MCU使能了下拉电阻,导致本应该为高电平的时候高不上去,把上拉电阻降低为4.7kΩ满足电平要求。涉及此管脚输出低电平时内部MOS管的电流流通能力,所以烦请确认下此方案是否可行,谢谢。

  • 您好, ID 是输出引脚,和MCU的哪个管脚接在一起了? 不需要接在一起呢。它后端也不需要驱动device,所以电流驱动能力我觉得影响不大。
    它只是在DFP,DRP模式下检测CC pin上是否有device。 UFP模式下不需要。