Other Parts Discussed in Thread: TXB0104, SN74AXC4T774
使用TXS0108 , 將VCCA接1.8 or 3.3V; VCCB接3.3v
有無附載的狀況下,輸入4Mhz的CLK, b端輸出震幅只有左右0~1.9v
嘗試PULL UP電阻1.8k, 輸出震幅可達0.3~2.4v
但是還不是不足預期的3v左右
請問是我輸入的Rise / fall rate的問題嗎? 10ns/V???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0104, SN74AXC4T774
使用TXS0108 , 將VCCA接1.8 or 3.3V; VCCB接3.3v
有無附載的狀況下,輸入4Mhz的CLK, b端輸出震幅只有左右0~1.9v
嘗試PULL UP電阻1.8k, 輸出震幅可達0.3~2.4v
但是還不是不足預期的3v左右
請問是我輸入的Rise / fall rate的問題嗎? 10ns/V???
您好,参考datasheet 6.5部分的电气参数表,TXS0108的输出Voh=VccA(VccB)*0.67V , 所以当VCCB=3.3V的时候 Voh=2.2V。
如果输出高电平达到3V左右,建议使用带方向控制SN74xx的电平转换器件。
感謝回復
但是我看CLK大概2V,但是CS or MO, MI 都還能到3v左右
如果都是參考vccbx0.67 應該是要一致的
我量測了input 的rise time約1v/25ns
spec是10ns/1v
需要再10ns以內嗎??