This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H硬件配置成RMII主模式可以ping通,去掉硬件配置用软件配置寄存器方式无法ping通,是什么原因?



软件寄存器0X0017 我配成0X0065(此值是硬件可ping通情况下查询值), RX_D3引脚没有50Mhz时钟参考,硬件配置引导模式就有,请问此种问题出现在哪里,帮忙解答,谢谢!

  • 您好,0X0017 bit6配置为0试试呢? 您这里配置的0X0065, 其中bit 6=1 normal operation。
    默认为0 = Bypass Asynchronous FIFO。When in RMII Recovered Clock mode, the asynchronous FIFO can be bypassed to reduce the receive path latency within the DP83822. 50-MHz clock is outputted on RX_CLK when in Async fifo bypass 。
    这里描述,当配置为Async fifo bypass模式时候,RX_CLK会有 50Mhz输出。
  • 你好请问可以 提供一下你使用的驱动和原理图吗?