因为设计需要,本人现在需要用SN74AVC4T245将1.8V的SPI总线信号与3.3V的主芯片SPI接口进行通信,有几个问题:
1.在1.8V的输出口是否还需要上拉电阻,来稳定SPI输出口的起始状态?
2.时钟信号通过SN74AVC4T245,是否会出现问题?
3.是否有更好的替代方案?
谢谢大家了!!!感激不及!!!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为设计需要,本人现在需要用SN74AVC4T245将1.8V的SPI总线信号与3.3V的主芯片SPI接口进行通信,有几个问题:
1.在1.8V的输出口是否还需要上拉电阻,来稳定SPI输出口的起始状态?
2.时钟信号通过SN74AVC4T245,是否会出现问题?
3.是否有更好的替代方案?
谢谢大家了!!!感激不及!!!

首先SN74AVC4T245可以实现1.8到3.3V电平转换,也可以应用在SPI总线上。
1.不需要外接上拉电阻。
2.1.8V~3.3V转换时,最大data rate为380Mbps(190MHz)。所以时钟信号不超过这个值是可以的。
3.还可以选择TXS0104E,不带方向控制位,应用起来更便捷。