This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571 I2S mode频率调整范围以及VCO的输出校准



1.看到芯片有校准的功能,这个是在上电的时候校准一次就好了么,还是说每次切换VCO都要校准?

2.想得到FM的chirp连续频率变化的输出,如果要跨越两个VCO,需要校准么?可以设置不校准么?

3.在I2S模式或者SPIfast模式下直接配置输出频,这个时候可以直接改输出分频CHDIV1 和CHDIV2

的么?可以的话,输出会直接跳到对应的频率还是说会怎么样?这个稳定时间大概是多少?

  • 您好,
    只有当需要改变VCO的频率时,才需要进行VCO校准。
    总锁定时间包括(1)编程时间(2)VCO校准时间和(3)模拟环路锁定时间。
    如果在切换到新的VCO频率时需要改变输出分频器,那么由于寄存器写入时间增加,只有(1)会更长。
    如果频率变化仅仅是由于输出分频器值的改变,则不涉及“锁定时间”,只需对分频器寄存器进行编程即可。分频器的响应时间很快,在ns范围内