Other Parts Discussed in Thread: AFE5808
请问有1.8V LVDS标准逻辑电平转3.3V LVDS或者COMS的逻辑电平的芯片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE5808
请问有1.8V LVDS标准逻辑电平转3.3V LVDS或者COMS的逻辑电平的芯片吗?
您好,LVDS的高电平为1.4V, 低电平为1V,共模电压为1.2V, 幅值为400mV。
所以您这里提到的1.8V LVDS和3.3V LVDS,没有这种电平转换器件。
具体是什么信号?
我使用的芯片是AFE5808,ADC输出的LVDS信号就是共模1.1V,幅值400mV,ADC输出的LVDS连接到Spartan-6,Spartan-6的电平标准是LVDS_33,原语转换成单端信号之后,使用ChipScope抓取的波形是乱的,我怀疑是LVDS电平不匹配导致的。