This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2581E无输出

Other Parts Discussed in Thread: LMX2581E, LMX2581

电路原理图如上,用示波器可以测到U32(LMX2581E)的第20管脚OSCIN有100MHz时钟信号,然后对LMX2581E的寄存器进行配置,

配置完以上寄存后,用频谱分析仪测试LMX2581E的第12管脚RFOUTA+,测不到2.5GHz频率输出。

请问对这个LMX2581E的配置或者电路原理图哪里有问题?

  • 您好,我看寄存器R15 OUT_LDEN 位配置的为0, 建议将其配置为1, 然后通过PLL锁存状态,判断LMX2581 输出是否disable。
    RFOUT这里没有输出,应该是PLL没有lock. 可以读一下寄存器R13. R13 是针对PLLlock状态的一个监测。
    另外,就是建议参考下8.5.2 Recommended Initial Power on Programming Sequence部分的初始化顺序:
    www.ti.com.cn/.../lmx2581e.pdf