您好:
FPGA侧电平是1.8V,但是Ethernet PHY侧信号是3.3V,想找个双向电压转换的芯片。我看到LSF0108最大可以满足200MHz,想问下我能不能使用?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
FPGA侧电平是1.8V,但是Ethernet PHY侧信号是3.3V,想找个双向电压转换的芯片。我看到LSF0108最大可以满足200MHz,想问下我能不能使用?
谢谢!
您好,这是LSF0108 能够支持的频率。容性负载小于30pF的时候,升压电平转换能支持到100Mhz,降压转换能支持到低于100Mhz,当容性负载在50pF的时候只能支持到40Mhz。
Supports up to 100-MHz up translation and greater than 100-MHz down translation at ≤ 30pF cap load and up To 40-MHz up/down translation at 50pF cap load
建议您使用带方向控制位的SN74xx系列的电平转换,驱动能力也强一些,您需要8bit的吗?
嗯嗯,我也看到啦带方向控制的芯片,但是那样的话,我FPGA那边还需要实施考虑方向检测。想用个硬件上可控的器件,LSF0108怎么去算容性负载这个是不是小于30pF还是50pF呢?或者您有其他的推荐吗?不采用方向的。4bit/8bit或者16bit都可以。
多谢回复。我还是选择带dir方向的器件,负载电容比较大。LSF的不保证支持。而且RMII接口算下来,双向的主要就MDIO,其他都是单向的,选择带方向的比较稳妥些。