This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

74LVC161284使用问题

本人需要用到计算机并口做些通讯,刚开始搞,菜鸟一个,请各位大侠帮助

请问:1、B口是和主机口相连?如果我单片机是3.3V的,需要和计算机并口通讯,74lvc VCC CABLE供3。3V的可以么?(因为并口出来的是5V,但可以忍受3.3V?)

            2、如果我用DB25接口,单片机如何通过74lvc161284知道电脑并口是LEVEL1或者LEVEL2呢?如果是LEVEL1是不是通过HD选择相应脚通过带上拉的开漏通讯?如果是LEVEL2是不是都可以通过图腾柱方式通讯的呢?

问题有点小多,小繁琐,希望大侠多多帮助,准备画板做了,这些不搞懂不好画板的